IGBT: Cres Test

Measures the Reverse transfer capacitance. Requires the N1272A Device Capacitance Selector SMU.

Used with:

  • B1506A: IGBT DUT
  • B1505A: IGBT DUT, CV test type
Set the test parameters based on the specifications in the device's data sheet:
- If the data sheet lists a maximum test limit for a parameter, use that value.
- If there is no maximum test limit, use a typical value.

See also Setting IV and CV Test Parameters.

Test Schematic

Gate Parameters

Collector Parameters